4.1.2 DDR2-SDRAM Initialization

The initialization sequence is generated by software. The DDR2-SDRAM devices are initialized by the following sequence:

Table 4-2. DDR2-SDRAM Initialization
StepActionRegisterSetting
1Program the memory device typeMPDDRC_MDMD = 6 (for DDR2), DBW = 0 (32 bits)
2Program the shift sampling valueMPDDRC_RD_DATA_PATHSection SDRAM Controller Configuration provides values for these fields. These values depend on the DDR clock.
3Program DDR2-SDRAM featuresMPDDRC_CR MPDDRC_TPR0

MPDDRC_TPR1

MPDDRC_TPR2

4Issue a NOP command(4)MPDDRC_MRMODE = 1
5200 μs delay(1)––
6Issue a NOP command(4)MPDDRC_MRMODE = 1
7Issue an All Banks Precharge command(4)MPDDRC_MRMODE = 2
8Issue an EMRS2 cycle(2)MPDDRC_MRMODE = 5
9Issue an EMRS3 cycle(2)MPDDRC_MRMODE = 5
10Issue an EMRS1 cycle(2)MPDDRC_MRMODE = 5
112 μs delay(1)––
12Write a ‘1’ to the DLL bitMPDDRC_CRDLL = 1
13Issue a Mode Register Set (MRS) cycle(3)MPDDRC_MRMODE = 3
14Issue an All Banks Precharge command(4)MPDDRC_MRMODE = 2
15Provide two autorefresh (CBR) cycles(4)MPDDRC_MRMODE = 4
16Write a ‘0’ to the DLL bitMPDDRC_CRDLL = 0
17Issue a Mode Register Set (MRS) cycle(3)MPDDRC_MRMODE = 3
18Configure the OCD field to 7MPDDRC_CROCD = 7
19Issue an EMRS1 cycle(2)MPDDRC_MRMODE = 5
20Configure the OCD field to 0MPDDRC_CROCD = 0
21Issue an EMRS1 cycle(2)MPDDRC_MRMODE = 5
22Provide a Normal Mode command(4)MPDDRC_MRMODE = 0
23Write the refresh rate in COUNT fieldMPDDRC_RTRCOUNT = Trefi/Tck
Note:
  1. To issue a delay:

    • disable interrupts;

    • compute a deadline = ROUND_INT_DIV((timer_channel_freq/1000)*count, 1000), where count is the delay in µs;
    • start a timer and wait for the timer to reach the deadline;
    • enable interrupts.
  2. To issue an Extended Mode Register Set (EMRS) cycle, after setting the MODE field to 5, read MPDDRC_MR and add a memory barrier assembler instruction just after the read. Then perform a write access to the DDR2-SDRAM device so that the BA[1:0] signals are as follows:

    • BA[1] is set to 0, BA[0] is set to 1 for EMRS1;
    • BA[1] is set to 1, BA[0] is set to 0 for EMRS2;
    • BA[1] is set to 1, BA[0] is set to 1 for EMRS3.

      The address at which the write access is issued in order to acknowledge the command needs to be calculated so that the BA[1:0] signals are in the right state for an EMRS cycle.

  3. After setting the MODE field, read MPDDRC_MR and add a memory barrier assembler instruction just after the read. Perform a write access to acknowledge the command so that BA[2:0] signals are set to 0 (write at BASE_ADDRESS_DDR).
  4. After setting the MODE field, read MPDDRC_MR and add a memory barrier assembler instruction just after the read. Perform a write access at any address to acknowledge the command.


Refer to chapter ”Multiport DDR-SDRAM Controller (MPDDRC)” of the SAMA5D2 Series data sheet for more information.