41.6.2.6 Double Buffering
The Pattern (PATT), Period
(PER) and Compare Channels (CCx) registers are all double buffered. Each buffer register
has a buffer valid (PATTBUFV, PERBUFV and CCBUFVx) bit in the STATUS register that
indicates that the Buffer register contains a valid value that can be copied into the
corresponding register. As long as the
respective Buffer Valid Status flags (PATTBUFV, PERBUFV or CCBUFVx) are set to ‘1’,
the related SYNCBUSY bits are set (SYNCBUSY.PATT, SYNCBUSY.PER or SYNCBUSY.CCx), a write to the respective
PATT/PATTBUF, PER/PERBUF or CCx/CCBUFx registers will generate a PAC error,
and read access to the respective PATT, PER or CCx register is invalid.
1’ and the Lock
Update bit in the CTRLB register is set to ‘0’ (writing CTRLBCLR.LUPD to
‘1’), double buffering is enabled: the data from the buffer registers
will be copied into the corresponding register under the hardware UPDATE conditions, then
the Buffer Valid flags bit in the STATUS register is automatically cleared by the hardware.
Both the registers (PATT/PER/CCx) and
corresponding Buffer registers
(PATTBUFPERBUF/CCBUFx) are available in the I/O register map, and the
double buffering feature is not mandatory. The double buffering is disabled by writing a
‘1’ to CTRLSET.LUPD.
Changing the Period
The counter period can be changed by writing a new Top value to the Period register (PER or CC0, depending on the Waveform Generation mode). Any period update on the registers (PER or CCx) is effective after the synchronization delay, whatever double buffering enabling is.
A counter wraparound can occur in any operation mode when up-counting without buffering (see Figure 41-10). COUNT and TOP are continuously compared, so when a new value that is lower than the current COUNT is written to TOP, COUNT will wrap before a compare match.
When double buffering is used, the buffer can be written at any time and the counter will still maintain correct operation. The period register is always updated on the update condition, as shown in Figure 41-13. This prevents wraparound and the generation of odd waveforms.