17.3 Block Diagram
The following figure shows the block diagram of the Deadman Timer.
Note:
- The DMT Max Count is controlled by the DMTCNT[4:0] bits in the CFGCON2 register “Maximum = 2^31”.
- The DMT Window Interval is controlled by the DMTINTV[2:0] bits in the CFGCON2 register.
- For more details, see Resets from Related Links.