8.3 Command Format
Most CryptoMemory® commands have the same format as a Two-Wire Interface (TWI) write command, characterized by a zero in the LSB of the first byte (device address). The only exception is the Random Read command, which has a one in the LSB of the device address byte.