8.11.2 Read Config Zone
The data byte address to be read is defined by Address 2 in the command and is internally incremented following the transmission of each data byte. The value N defines how many bytes CryptoMemory® will read; a value of zero will result in 256 bytes read. If the address provided is unauthorized, the device will not ACK the N byte and will not return any data. Since access rights vary throughout the Configuration zone, the host may provide an authorized starting address and a number of bytes N that causes the device to reach unauthorized data. In this case, the device will transmit the fuse byte (see below) in place of unauthorized bytes.