8.10.4 Set User Zone

Before reading and writing data in the user zones, the host must select a zone with this command. At this time, the host chooses whether anti-tearing will be active for this zone.

Table 8-5. Anti-Tearing

Command Description

Command

Addr 1

Addr 2

N

Data(N)

Write Config Zone with Anti-Tearing

$B4

$08

Addr

N ≤ $08

N bytes

Set User Zone with Anti-Tearing

$B4

$0B

Zone

$00

Data written to the Configuration zone may be done with anti-tearing enabled by setting Address 1 to $08 of the write Configuration zone command.

To enable anti-tearing for writes to a user zone, a Set User Zone command is executed with Address 1 set to $0B. All subsequent Write User Zone commands will be executed with anti-tearing enabled until the next Set User Zone command. Anti-tearing must be turned off if not required, as it would otherwise cause more write cycles than necessary.
Figure 8-12. System Write Command Detail
???