5.9.2.4 Monitor Security Network ARP Inspection
Entries in the Dynamic ARP Inspection Table are shown on the Dynamic ARP Inspection Table page. The Dynamic ARP Inspection Table contains up to 256 entries, and is sorted first by port, then by VLAN ID, then by MAC address, and then by IP address. All dynamic entries are learning from DHCP Snooping.

The Dynamic ARP Inspection Table page has the following parameters:
- Port: Switch Port Number for which the entries are displayed
- VLAN ID: VLAN-ID in which the ARP traffic is permitted
- MAC Address: User MAC address of the entry
- IP Address: User IP address of the entry