4.6 ERPS Configuration
The ERPS instances are configured on the ERPS Configuration page. See the following figure.
The ERPS Configuration page has the following parameters:
- Configuration:
- ERPS #: The ID of ERPS. The allowed value is from 1:64.
- Version: ERPS protocol version. v1 and v2 are supported.
- Type: Type of ring. The
following are the possible values:
- Major: ERPS major ring (G.8001-2016, clause 3.2.39)
- Sub: ERPS sub-ring (G.8001-2016, clause 3.2.66)
- InterSub: ERPS sub-ring on an interconnection node (G.8001-2016, clause 3.2.66)
- VC: Controls whether to use a Virtual Channel with a sub-ring
- Interconnect Instance: For a sub-ring on an interconnection node, this must refer the instance ID of the ring to which this sub-ring is connected.
- Interconnect Prop: Controls whether the ring referenced by Interconnect Instance shall propagate R-APS flush PDUs whenever this sub-ring's topology changes.
- Ring ID: The Ring ID is used. Along with the control VLAN, this is used to identify R-APS PDUs as belonging to a particular ring.
- Node ID: The Node ID is used inside the R-APS specific PDU to uniquely identify this node (switch) on the ring
- Level: MD/MEG Level of R-APS PDUs that are transmitted
- Control VLAN: The VLAN on which R-APS PDUs are transmitted and received on the ring ports
- Control PCP: The PCP value used in the VLAN tag of the R-APS PDUs
- Rev: Revertive (true) or Non-Revertive (false) mode
- Guard: Guard time in ms. The valid range is 10 ms–2000 ms
- WTR: Wait-to-Restore time in seconds. Valid range 1s–720s
- Hold Off: Hold off time in ms. Value is rounded down to 100 ms precision. Valid range is 0 ms–10000 ms.
- Enable: The administrative state of this ERPS. Check to make it function normally and uncheck to make it stop functioning.
- Signal Fail Trigger
- Type: Selects whether Signal Fail (SF) comes from the link state of a given interface or from a Down-MEP.
- Domain, Service, MEPID: Identification of the MEP instance to provide SF, if Type is MEP.
- Protected VLANs: VLANs, which are protected by this ring instance. At least one VLAN must be protected. Specify as a comma-separated list of VLAN numbers or VLAN ranges. For example, 1, 4, 7, 30–70.
- Ring Protection Link:
- RPL Mode: The following
Ring Protection Link modes are available:
- None: This switch does not have the RPL port in the ring
- Owner: This switch is RPL owner for the ring (G.8001-2016, clause 3.2.61)
- Neighbor: This switch is RPL neighbor for the ring (G.8001-2016, clause 3.2.60)
- RPL Port: Allows you to select the east (port 0) or west (port 1) as the RPL block. This is not used if the RPL mode is None.
- RPL Mode: The following
Ring Protection Link modes are available: