BLE_GAP_SetScanningParam

C

uint16_t BLE_GAP_SetScanningParam(BLE_GAP_ScanningParams_T *p_scanParams);

Description

Sets the scanning parameters.

Note

This API should not be called while scanning is active. It is part of the legacy advertising feature set and will be disallowed if any API from the extended advertising feature set has been used previously. See BLE_GAP_ADV_CATS for details on advertising APIs. The BLE_GAP_ScanInit function must be called prior to using this API.

Parameters

ParameterDescription
[in] p_scanParamsPointer to a BLE_GAP_ScanningParams_T structure containing the desired scanning parameters.

Return values

Return valueDescription
MBA_RES_SUCCESSSuccessfully sets scanning parameters.
MBA_RES_OOMInternal memory allocation failure occurred.
MBA_RES_INVALID_PARAInvalid parameters, such as out-of-range scanning parameters.
MBA_RES_COMMAND_DISALLOWEDCommand disallowed when the extended advertising feature is in use.