BLE_GAP_SetExtAdvParams
C
uint16_t BLE_GAP_SetExtAdvParams(BLE_GAP_ExtAdvParams_T *p_extAdvParams, int8_t *p_selectedTxPower);
Description
Configures the extended advertising parameters.
Note
This API is part of the extended advertising feature and is disallowed if any legacy advertising feature API has been used prior. See BLE_GAP_ADV_CATS for advertising API details. Initialization with BLE_GAP_AdvInit or BLE_GAP_ExtAdvInit is required before calling this API. When using coded PHY, the default coding scheme is S=8 (S: Transmitted Symbols). Use BLE_GAP_SetExtAdvCodingScheme to change the coding scheme.
If legacy advertising PDU types are being used and the advertising set already contains data, the type shall be one that supports advertising data, and the amount of data shall not exceed 31 bytes.
If extended advertising PDU types are being used, then:
The advertisement shall not be both connectable and scannable.
High duty cycle directed connectable advertising shall not be used (bit 3 = 0).
This API only accepts 2 configurations from the 2nd advertising set:
Event property is non-connectable and non-scannable: This advertising set will use Non-RPA automatically and change periodically. The default address timeout is 15 minutes if the application has not set local privacy via BLE_GAP_SetLocalPrivacy.
Event property is connectable or scannable: The peer address must be in the resolving list and local privacy must be enabled. This peer address should not use the same IRK as other advertising sets. This advertising set will use RPA.
It is recommended to clear and reconfigure all advertising sets after calling BLE_GAP_SetLocalPrivacy or BLE_GAP_SetResolvingList due to potential changes in privacy settings.
Parameters
Parameter | Description |
---|---|
[in] p_extAdvParams | Pointer to the structure containing extended advertising parameters. See BLE_GAP_ExtAdvParams_T. |
[out] p_selectedTxPower | Pointer to the variable where the selected transmit power level will be stored. (Unit: dBm) |
Return values
Return value | Description |
---|---|
MBA_RES_SUCCESS | Successfully configures the extended advertising parameters. |
MBA_RES_OOM | Internal memory allocation failure occurred. |
MBA_RES_INVALID_PARA | The parameters provided are invalid. |
MBA_RES_COMMAND_DISALLOWED | Command disallowed due to a conflicting operation or state. |