BLE_GAP_SetPhy

C

uint16_t BLE_GAP_SetPhy(uint16_t connHandle, uint8_t txPhys, uint8_t rxPhys, uint8_t phyOptions);

Description

Sets the PHY preferences for the specified connection.

Note

The BLE Stack might not be able to make the change immediately. An event will be generated if one or both PHYs change.

Events generated

BLE_GAP_EVT_PHY_UPDATE is generated when the PHY is updated.

Return values

Return valueDescription
MBA_RES_SUCCESSSuccessfully sets the PHY preferences for the specified connection.
MBA_RES_OOMInternal memory allocation failure occurred.
MBA_RES_INVALID_PARAThe parameters provided are invalid.
MBA_RES_UNKNOWN_CONN_IDUnknown connection identifier.
MBA_RES_COMMAND_DISALLOWEDCommand disallowed due to a conflicting operation or state.