BLE_GAP_SetDeviceAddr
C
uint16_t BLE_GAP_SetDeviceAddr(BLE_GAP_Addr_T *p_addr);
Description
Sets the Bluetooth device address (identity address).
Note
The address type must be either Address types_PUBLIC or Address types_RANDOM_STATIC. The address identifies the device to other Bluetooth devices. The default IRK (Identity Resolving Key) is automatically changed if the Bluetooth device address is updated.
Parameters
Parameter | Description |
---|---|
[in] p_addr | Pointer to the device address buffer. See BLE_GAP_Addr_T. |
Return values
Return value | Description |
---|---|
MBA_RES_SUCCESS | Successfully sets the device address. |
MBA_RES_FAIL | Failed to set device address due to invalid address type or other conditions. |
MBA_RES_OOM | Internal memory allocation failure occurred. |