BLE_GAP_TerminateSync
C
uint16_t BLE_GAP_TerminateSync(uint16_t syncHandle);
Description
Stops reception of the periodic advertising train identified by the provided syncHandle.
Note
This API is part of the extended advertising feature set and is not compatible with legacy advertising APIs. See BLE_GAP_ADV_CATS for details. Initialization with BLE_GAP_ScanInit, BLE_GAP_ExtScanInit, and BLE_GAP_SyncInit is required before using this API.
Parameters
Parameter | Description |
---|---|
[in] syncHandle | Identity of the periodic advertising train. Range: 0x0000 to 0x0EFF. |
Return values
Return value | Description |
---|---|
MBA_RES_SUCCESS | Successfully stops reception of the periodic advertising train. |
MBA_RES_OOM | Internal memory allocation failure occurred. |
MBA_RES_COMMAND_DISALLOWED | Command disallowed due to a conflicting operation or state. |
MBA_RES_UNKNOWN_ADV_ID | Unknown advertising identifier. |