3.2.1 Recovery Method
When the MPLAB PKOB4 is unresponsive, use the MPLAB X IDE tool to recover the WFI32-IoT board through the following recovery method:
- Short the pin1 and pin2 of the
connector (J301) to the ground for approximately 15 seconds; see the following
figure.Note: Ensure that the WFI32-IoT board is turned ON to perform the recovery method.
Figure 3-3. WFI32-IoT Board (EV36W50A) – Recovery Method - Open the latest version of MPLAB X IDE.
- The following figure illustrates the
opening window of the MPLAB X IDE. From the “Debug” drop-down list, select
Hardware Tool Emergency Boot Firmware Recovery.
Figure 3-4. MPLAB® X IDE Opening Window - Follow the instructions shown in the preceding figure to bring the tool back to factory condition. For additional information on the MPLAB PKOB4, refer to the MPLAB® PICkit™ 4 In-Circuit Debugger User's Guide (DS50002751) and MPLAB Snap In-Circuit Debugger User's Guide (DS50002787).