38.6.2.11 Management of Control Endpoints
Overview
A SETUP request is always ACKed. When a new SETUP packet is received, the USBHS_DEVEPTISRx.RXSTPI is set; the Received OUT Data Interrupt (USBHS_DEVEPTISRx.RXOUTI) bit is not.
The FIFO Control (USBHS_DEVEPTIMRx.FIFOCON) bit and the Read/Write Allowed (USBHS_DEVEPTISRx.RWALL) bit are irrelevant for control endpoints. The user never uses them on these endpoints. When read, their values are always zero.
Control endpoints are managed using these bits:
- The USBHS_DEVEPTISRx.RXSTPI bit, which is set when a new SETUP packet is received and which is cleared by firmware to acknowledge the packet and to free the bank.
- The USBHS_DEVEPTISRx.RXOUTI bit, which is set when a new OUT packet is received and which is cleared by firmware to acknowledge the packet and to free the bank
- The Transmitted IN Data Interrupt (USBHS_DEVEPTISRx.TXINI) bit, which is set when the current bank is ready to accept a new IN packet and which is cleared by firmware to send the packet
Control Write
The following figure shows a control write transaction. During the status stage, the controller does not necessarily send a NAK on the first IN token:
- If the user knows the exact number of descriptor bytes that must be read, it can then anticipate the status stage and send a zero-length packet after the next IN token, Or
- It can read the bytes and wait for the NAKed IN Interrupt
(USBHS_DEVEPTISRx.NAKINI), which acknowledges that all the bytes have been sent by the
host and that the transaction is now in the status stage.
Figure 38-9. Control Write
Control Read
The following figure shows a control read transaction. The USBHS has to manage the simultaneous write requests from the CPU and the USB Host.
A NAK handshake is always generated on the first status stage command.
When the controller detects the status stage, all data written by the CPU is lost and clearing USBHS_DEVEPTISRx.TXINI has no effect.
The user checks if the transmission or the reception is complete.
The OUT retry is always ACKed. This reception sets USBHS_DEVEPTISRx.RXOUTI and USBHS_DEVEPTISRx.TXINI. Handle this with the following software algorithm:
- Set TXINI
- Wait for RXOUTI OR TXINI
- If RXOUTI, then clear bit and return
- If TXINI, then continue
Once the OUT status stage has been received, the USBHS waits for a SETUP request. The SETUP request has priority over any other request and has to be ACKed. This means that any other bit should be cleared and the FIFO reset when a SETUP is received.
The user must consider that the byte counter is reset when a zero-length OUT packet is received.