22.6.1 Divider and Phase Lock Loop Programming
The divider can be set between 1 and 255 in steps of 1. When a divider field (DIV) is cleared, the output of the corresponding divider and the PLL output is a continuous signal at level 0. On reset, each DIV field is cleared, thus the corresponding PLL input clock is stuck at ‘0’.
The PLL (PLLA) allows multiplication of the divider’s outputs. The PLL clock signal has a frequency that depends on the respective source signal frequency and on the parameters DIV (DIVA) and MUL (MULA). The factor applied to the source signal frequency is (MUL + 1)/DIV. When MUL is written to ‘0’ or DIV = 0, the PLL is disabled and its power consumption is saved. Note that there is a delay of two SLOW_CLK clock cycles between the disable command and the real disable of the PLL. Re-enabling the PLL can be performed by writing a value higher than ‘0’ in the MUL field and DIV higher than ‘0’.
Whenever the PLL is re-enabled or one of its parameters is changed, the LOCK (LOCKA) bit in PMC_SR is automatically cleared. The values written in the PLLCOUNT field (PLLACOUNT) in CKGR_PLLR (CKGR_PLLAR) are loaded in the PLL counter. The PLL counter then decrements at the speed of SLOW_CLK until it reaches ‘0’. At this time, PMC_SR.LOCK is set and can trigger an interrupt to the processor. The user has to load the number of SLOW_CLK cycles required to cover the PLL transient time into the PLLCOUNT field.
To avoid programming the PLL with a multiplication factor that is too high, the user can saturate the multiplication factor value sent to the PLL by setting the PLLA_MMAX field in the PLL Maximum Multiplier Value Register (PMC_PMMR).
It is forbidden to change the MAINCK characteristics (oscillator selection, frequency adjustment of the Main RC oscillator) when:
- MAINCK is selected as the PLLA clock source
- MAIN_CLK is sourced from the PLLA
To change the MAINCK characteristics, the user must perform these actions:
- Switch the MAIN_CLK source to MAINCK by writing a ‘1’ to PMC_MCKR.CSS.
- Change the Main RC oscillator frequency (MOSCRCF) or oscillator selection (MOSCSEL) in CKGR_MOR.
- Wait for MOSCRCS (if frequency changes) or MOSCSELS (if oscillator selection changes) in PMC_SR.
- Disable and then enable the PLL.
- Wait for the LOCK flag in PMC_SR.
- Switch back MAIN_CLK to the PLLA by writing the appropriate value to PMC_MCKR.CSS.