39.10.4 CE-ATA Error Recovery
Several methods of ATA command failure may occur, including:
- No response to an MMC command, such as RW_MULTIPLE_REGISTER (CMD60)
- CRC is invalid for an MMC command or response
- CRC16 is invalid for an MMC data packet
- ATA Status register reflects an error by setting the ERR bit to one
- The command completion signal does not arrive within a host specified time out period
Error conditions are expected to happen infrequently. Therefore, a robust error recovery mechanism may be used for each error event. The recommended error recovery procedure after a timeout is:
- Issue the command completion signal disable if nIEN was cleared to zero and the RW_MULTIPLE_BLOCK (CMD61) response has been received
- Issue STOP_TRANSMISSION (CMD12) and successfully receive the R1 response
- Issue a software reset to the CE-ATA device using FAST_IO (CMD39)
If STOP_TRANMISSION (CMD12) is successful, then the device is again ready for ATA commands. However, if the error recovery procedure does not work as expected or there is another timeout, the next step is to issue GO_IDLE_STATE (CMD0) to the device. GO_IDLE_STATE (CMD0) is a hard reset to the device and completely resets all device states.
Note that after issuing GO_IDLE_STATE (CMD0), all device initialization needs to be completed again. If the CE-ATA device completes all MMC commands correctly but fails the ATA command with the ERR bit set in the ATA Status register, no error recovery action is required. The ATA command itself failed implying that the device could not complete the action requested, however, there was no communication or protocol failure. After the device signals an error by setting the ERR bit to one in the ATA Status register, the host may attempt to retry the command.