24.4.5.1.3 Handling the GETSTATUS CCC

The supported format for the GETSTATUS CCC is shown in Figure 24-34.

Figure 24-34. Handling of the GETSTATUS CCC
A screenshot of a computer AI-generated content may be incorrect.

The GETSTATUS vendor-reserved fields are used to indicate the error conditions that have occurred in the previous transfer. In case of any error, the next private transfer coming from the Controller is NACKed. The Controller can understand the status of the transfer, which is not successfully accepted or transmitted, by issuing the GETSTATUS CCC.

The I3CxTGTCCCSTAT register reflects all the information passed to the Controller when the Controller issues the GETSTATUS CCC.

A detailed description of the error fields and other status fields present in the GETSTATUS CCC format supported is provided in the description of the I3CxTGTCCCSTAT register.