13.2.3 Clipboard Toolbar
The Clipboard toolbar currently contains button icons for the following functions. These functions are also on the Edit menu.
| Icon | Icon Text | Function |
|---|---|---|
![]() | Cut | Deletes the current selection and places it on the clipboard. |
![]() | Copy | Copies the current selection to the clipboard. |
![]() | Paste | Pastes the contents of the clipboard into the insertion point. |