3.4.9.1 Obtain the Manufacturer UUID from Microchip
Manufacturer UUID (M_UUID) is a 40-symbol hex string identifier that is assigned by Microchip through the Microchip Portal (see the Secure Production Programming Solution (SPPS) User Guide for details).
Example of the Manufacturer UUID: 0000000000000000000000000000000000000002
Note: UUID must have all lower-case
characters.
Private/Public SEE keys must use the Manufacturer UUID assigned by Microchip.
Once the UUID value is available, update the tag in both M-HSMMaster.config files, under the Server and Tools directories, as explained in section Update Server and Tools Configuration File.