3.6.8.5 FPU and CPU Exceptions

Issued FPU instructions that become committed (accepted by the Execute stage) are always atomic with respect to CPU exceptions. No CPU exception (other than a Reset event) can force the FPU to abandon an instruction that is already underway.

CPU exceptions will result in a register context switch in both the CPU and FPU. Furthermore, FPU exceptions are always context specific. That is, any FPU exception occurring after a context switch will remain pending until the FPU returns to the prior context.

FPU exceptions can only be taken and handled when unmasked (referred to as alternate exception handling). The FPU will return the calculated result of each operation and signal any exception via an interrupt to the CPU.

If FPU exceptions are masked, the FPU will return a default result for each operation that generates an exception as defined in Table 3-15 . The exception will be signaled by setting the corresponding bit(s) in the FSR, but no interrupt will be issued to the CPU. This is intended to allow code to execute unhindered by exception handling at the time of execution. If required, exception status may be examined at a later time and appropriate action will be taken.