Exception During Successful BOOTSWP Operation

If timing of an exception during BOOTSWP execution meets that outlined in Figure 6-4, and the BOOTSWP criteria are met, the panel swap will be completed by the time the interrupt or trap handler vector fetch commences (during BOOTSWP W stage). Exception processing will, therefore, vector into the newly active panel, and the handler will return to the address following the BOOTSWP in that panel.