5.11.2.1.4 Project Creation
In MPLAB X IDE, click the New Project button
and set up
a new stand-alone project.
and set up
a new stand-alone project.- Device: PIC32MX470F512H
- Tool: MPLAB ICE 4
- Compiler: MPLAB XC32 v2.50
In the new project, right click on “Source Files” in the Projects window and select new>main.c. Then enter the code below in the editor and save.
To produce current on the target board that is more than a single value, the target should be actively doing something. The following code for the target PIC32MX470F512H will flash LEDs on the board.
// PIC32MX470F512H Configuration Bit Settings
// 'C' source line config statements
// DEVCFG3
#pragma config USERID = 0xFFFF // Enter Hexadecimal value (Enter Hexadecimal value)
#pragma config FSRSSEL = PRIORITY_7 // Shadow Register Set Priority Select (SRS Priority 7)
#pragma config PMDL1WAY = ON // Peripheral Module Disable Configuration (Allow only one reconfiguration)
#pragma config IOL1WAY = ON // Peripheral Pin Select Configuration (Allow only one reconfiguration)
#pragma config FUSBIDIO = ON // USB USID Selection (Controlled by the USB Module)
#pragma config FVBUSONIO = ON // USB VBUS ON Selection (Controlled by USB Module)
// DEVCFG2
#pragma config FPLLIDIV = DIV_12 // PLL Input Divider (12x Divider)
#pragma config FPLLMUL = MUL_24 // PLL Multiplier (24x Multiplier)
#pragma config UPLLIDIV = DIV_12 // USB PLL Input Divider (12x Divider)
#pragma config UPLLEN = OFF // USB PLL Enable (Disabled and Bypassed)
#pragma config FPLLODIV = DIV_256 // System PLL Output Clock Divider (PLL Divide by 256)
// DEVCFG1
#pragma config FNOSC = FRCDIV // Oscillator Selection Bits (Fast RC Osc w/Div-by-N (FRCDIV))
#pragma config FSOSCEN = ON // Secondary Oscillator Enable (Enabled)
#pragma config IESO = OFF // Internal/External Switch Over (Disabled)
#pragma config POSCMOD = OFF // Primary Oscillator Configuration (Primary osc disabled)
#pragma config OSCIOFNC = OFF // CLKO Output Signal Active on the OSCO Pin (Disabled)
#pragma config FPBDIV = DIV_8 // Peripheral Clock Divisor (Pb_Clk is Sys_Clk/8)
#pragma config FCKSM = CSDCMD // Clock Switching and Monitor Selection (Clock Switch Disable, FSCM Disabled)
#pragma config WDTPS = PS1048576 // Watchdog Timer Postscaler (1:1048576)
#pragma config WINDIS = OFF // Watchdog Timer Window Enable (Watchdog Timer is in Non-Window Mode)
#pragma config FWDTEN = OFF // Watchdog Timer Enable (WDT Disabled (SWDTEN Bit Controls))
#pragma config FWDTWINSZ = WINSZ_25 // Watchdog Timer Window Size (Window Size is 25%)
// DEVCFG0
#pragma config DEBUG = OFF // Background Debugger Enable (Debugger is Disabled)
#pragma config JTAGEN = OFF // JTAG Enable (JTAG Disabled)
#pragma config ICESEL = ICS_PGx2 // ICE/ICD Comm Channel Select (Communicate on PGEC2/PGED2)
#pragma config PWP = OFF // Program Flash Write Protect (Disable)
#pragma config BWP = OFF // Boot Flash Write Protect bit (Protection Disabled)
#pragma config CP = OFF // Code Protect (Protection Disabled)
// #pragma config statements should precede project file includes.
// Use project enums instead of #define for ON and OFF.
#include <xc.h>
// Three LEDs: Red, Green, Yellow
#define LEDS_ON 0xD0
#define LEDS_OFF 0x00
void delay (void)
{
int n = 50000;
while(n>0) {n--;}
}
int main(void) {
// Port E access
TRISE = 0x0000; // set all port bits to be output
while(1) {
// delay value change
delay();
LATE = LEDS_ON; // write to port latch
// delay value change
delay();
LATE = LEDS_OFF; // write to port latch
}
return -1;
}