13.2.6.6.1 How to Configure the ITM
The following example describes how to output trace data in asynchronous trace mode.
- Configure the TPIU for asynchronous trace mode (see How to Configure the TPIU)
- Enable the write accesses into the ITM registers by writing 0xC5ACCE55 into the Lock Access Register (Address: 0xE0000FB0)
- Write 0x00010015 into the Trace Control Register:
- Enable ITM.
- Enable Synchronization packets.
- Enable SWO behavior.
- Fix the ATB ID to 1.
- Write 0x1 into the Trace Enable Register:
- Enable the Stimulus port 0.
- Write 0x1 into the Trace Privilege Register:
- Stimulus port 0 only accessed in privileged mode (Clearing a bit in this register will result in the corresponding stimulus port being accessible in user mode.)
- Write into the Stimulus port 0 register: TPIU (Trace Port Interface Unit). The TPIU acts as a bridge between the on-chip trace data and the ITM. It formats and transmits trace data off-chip at frequencies asynchronous to the core.