1.1.2.4.3 DRV_I2C_Open Function
C
DRV_HANDLE DRV_I2C_Open
(
const SYS_MODULE_INDEX drvIndex,
const DRV_IO_INTENT ioIntent
)Summary
Opens the specified I2C driver instance and returns a handle to it.
Description
This routine opens the specified I2C driver instance and provides a handle that must be provided to all other client-level operations to identify the caller and the instance of the driver. The ioIntent parameter defines how the client interacts with this driver instance.
Specifying a DRV_IO_INTENT_EXCLUSIVE will cause the driver to provide exclusive access to this client. The driver cannot be opened by any other client.
Precondition
Function DRV_I2C_Initialize must have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| drvIndex | Identifier for the object instance to be opened |
| ioIntent | Zero or more of the values from the enumeration DRV_IO_INTENT "ORed" together to indicate the intended use of the driver. See function description for details. |
Returns
If successful, the routine returns a valid open-instance handle (a number identifying both the caller and the module instance).
If an error occurs, the return value is DRV_HANDLE_INVALID. Error can occur
- if the number of client objects allocated via DRV_I2C_CLIENTS_NUMBER is insufficient.
- if the client is trying to open the driver but driver has been opened exclusively by another client.
- if the driver instance being opened is not initialized or is invalid.
- if the client is trying to open the driver exclusively, but has already been opened in a non exclusive mode by another client.
- if the driver is not ready to be opened, typically when the initialize routine has not completed execution.
Example
DRV_HANDLE handle;
handle = DRV_I2C_Open(DRV_I2C_INDEX_0, DRV_IO_INTENT_EXCLUSIVE);
if (handle == DRV_HANDLE_INVALID)
{
// Unable to open the driver
// May be the driver is not initialized or the initialization
// is not complete.
}Remarks
The handle returned is valid until the DRV_I2C_Close routine is called.