1.1.2.4.2 DRV_I2C_Status Function
C
SYS_STATUS DRV_I2C_Status( const SYS_MODULE_OBJ object)Summary
Gets the current status of the I2C driver module.
Description
This routine provides the current status of the I2C driver module.
Precondition
Function DRV_I2C_Initialize should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| object | Driver object handle, returned from the DRV_I2C_Initialize routine |
Returns
SYS_STATUS_READY - Initialization has succeeded and the I2C is ready for additional operations.
SYS_STATUS_UNINITIALIZED - Indicates that the driver is not initialized.
Example
SYS_MODULE_OBJ object; // Returned from DRV_I2C_Initialize
SYS_STATUS i2cStatus;
i2cStatus = DRV_I2C_Status(object);
if (i2cStatus == SYS_STATUS_READY)
{
// This means the driver can be opened using the
// DRV_I2C_Open() function.
}Remarks
A driver can be opened only when its status is SYS_STATUS_READY.