1.1.2.4.19 DRV_I2C_TRANSFER_EVENT Enum
C
typedef enum
{
/* Transfer request is pending */
DRV_I2C_TRANSFER_EVENT_PENDING = 0,
/* All data from or to the buffer was transferred successfully. */
DRV_I2C_TRANSFER_EVENT_COMPLETE = 1,
/* Transfer Handle given is expired. It means transfer
is completed but with or without error is not known. */
DRV_I2C_TRANSFER_EVENT_HANDLE_EXPIRED = 2,
/* There was an error while processing the buffer transfer request. */
DRV_I2C_TRANSFER_EVENT_ERROR = -1,
DRV_I2C_TRANSFER_EVENT_HANDLE_INVALID = -2
} DRV_I2C_TRANSFER_EVENT;
Summary
Identifies the possible events that can result from a buffer add request.
Description
This enumeration identifies the possible events that can result from a buffer add request caused by the client calling either the DRV_I2C_ReadTransferAdd, DRV_I2C_WriteTransferAdd or DRV_I2C_WriteReadTransferAdd functions.
Remarks
One of these values is passed in the "event" parameter of the event handling callback function that the client registered with the driver by calling the DRV_I2C_TransferEventHandlerSet function when a buffer transfer request is completed.