1.1.2.4.13 DRV_I2C_WriteTransfer Function
C
bool DRV_I2C_WriteTransfer(
const DRV_HANDLE handle,
uint16_t address,
void* const buffer,
const size_t size
)Summary
This is a blocking function that performs a I2C write operation.
Description
This function does a blocking write operation. The function blocks till the write is complete or error has occurred during write. Function will return false to report failure. The failure will occur for the following reasons:
- Invalid input parameters
Precondition
DRV_I2C_Open must have been called to obtain a valid opened device handle.
Parameters
| Param | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine DRV_I2C_Open function. |
| address | Slave Address |
| buffer | Source buffer containing data to be written. |
| size | Size in bytes of data to be written. |
Returns
true - write is successful
false - error has occurred
Example
uint8_t myTxBuffer[MY_TX_BUFFER_SIZE];
// myI2CHandle is the handle returned
// by the DRV_I2C_Open function.
// slaveAddress is address of I2C slave device
// to which data is to be written
if (DRV_I2C_WriteTransfer(myI2CHandle, slaveAddress, myTxBuffer, MY_TX_BUFFER_SIZE) == false)
{
// Error handling here
}
Remarks
This function is thread safe in a RTOS application. This function should not be called from an interrupt context. This function is available only in the synchronous mode.