1.2.5.4.2 SYS_DEBUG_Status Function
C
SYS_STATUS SYS_DEBUG_Status ( SYS_MODULE_OBJ object )
Summary
Returns status of the specific instance of the debug service module.
Description
This function returns the status of the specific debug service module instance.
Precondition
The SYS_DEBUG_Initialize function should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| object | Debug module object handle, returned from SYS_DEBUG_Initialize |
Returns
SYS_STATUS_READY - Indicates that the module is running and ready to service requests. Any value greater than SYS_STATUS_READY is also a normal running state in which the module is ready to accept new operations.
SYS_STATUS_BUSY - Indicates that the module is busy with a previous system level operation.
SYS_STATUS_ERROR - Indicates that the module is in an error state. Any value less than SYS_STATUS_ERROR is also an error state.
SYS_STATUS_UNINITIALIZED - Indicates that the module has not been initialized.
Example
SYS_MODULE_OBJ object; // Returned from SYS_CONSOLE_Initialize
SYS_STATUS debugStatus;
debugStatus = SYS_DEBUG_Status (object);
if (debugStatus == SYS_STATUS_READY)
{
// Debug service is initialized and ready to accept requests.
}Remarks
None.