1.2.5.4 Library Interface
Debug System Service library provides the following interfaces:
Functions
| Name | Description |
|---|---|
| SYS_DEBUG_Initialize | Initializes the global error level and specific module instance |
| SYS_DEBUG_Status | Returns status of the specific instance of the debug service module |
| SYS_DEBUG_ErrorLevelSet | Sets the global system error reporting level |
| SYS_DEBUG_ErrorLevelGet | Returns the global system Error reporting level |
| SYS_DEBUG_Redirect | Allows re-direction of debug system service to another console instance |
| SYS_DEBUG_ConsoleInstanceGet | Returns console instance used by debug system service |
Data types and constants
| Name | Type | Description |
|---|---|---|
| SYS_ERROR_LEVEL | Enum | System error message priority levels |
| SYS_DEBUG_INDEX_0 | Macro | Debug System Service index |
| SYS_DEBUG_MESSAGE | Macro | Prints a debug message if the system error level is defined at or lower than the level specified |
| SYS_DEBUG_PRINT | Macro | Formats and prints an error message if the system error level is defined at or lower than the level specified |
| SYS_DEBUG_BreakPoint | Macro | Inserts a software breakpoint instruction when building in Debug mode |