1.2.5.4.5 SYS_DEBUG_Redirect Function
C
bool SYS_DEBUG_Redirect(const SYS_MODULE_INDEX index)Summary
Allows re-direction of debug system service to another console instance
Description
This function re-directs calls to the Debug Service APIs to a different console instance.
Precondition
None.
Parameters
| Param | Description |
|---|---|
| index | The index of the console to re-direct the debug system service calls to |
Returns
True - If operation is successful
False - In case of failure
Example
// Re-direct debug system service calls to console index 1
if (SYS_DEBUG_Redirect(SYS_CONSOLE_INDEX_1) == true)
{
// SYS Debug output will now be re-directed to SYS Console Instance - 1
}Remarks
None.