DRV_SST38_ChipErase Function
C
bool DRV_SST38_ChipErase( const DRV_HANDLE handle )Summary
Erase entire SST38 flash memory.
Description
This function schedules a blocking chip erase operation of flash memory.
Preconditions
The DRV_SST38_Open() routine must have been called for the specified SST38 driver instance.
Parameters
| Param | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
Returns
true
- if the erase request is successfully sent to the flash
false
- if Write enable fails before sending sector erase command to flash
- if chip erase command itself fails
Example
DRV_HANDLE handle;
if(DRV_SST38_ChipErase(handle) == flase)
{
printf("Error handling here");
}Remarks
None.