DRV_SST38_Open Function
C
DRV_HANDLE DRV_SST38_Open( const SYS_MODULE_INDEX drvIndex, const DRV_IO_INTENT ioIntent )Summary
Opens the specified SST38 driver instance and returns a handle to it.
Description
This routine opens the specified SST38 driver instance and provides a handle.
This handle must be provided to all other client-level operations to identify the caller and the instance of the driver.
Preconditions
Function DRV_SST38_Initialize must have been called before calling this function.
The driver should be in ready state to accept the request. Can be checked by calling DRV_SST38_Status().
Parameters
| Param | Description |
|---|---|
| drvIndex | Identifier for the instance to be opened |
| ioIntent | Zero or more of the values from the enumeration DRV_IO_INTENT "ORed" together to indicate the intended use of the driver |
Returns
If successful, the routine returns a valid open-instance handle (a number identifying both the caller and the module instance).
If an error occurs, DRV_HANDLE_INVALID is returned. Errors can occur under the following circumstances:
- If the driver hardware instance being opened is not initialized.
Example
DRV_HANDLE handle;
handle = DRV_SST38_Open(DRV_SST38_INDEX);
if (DRV_HANDLE_INVALID == handle)
{
printf("Unable to open the driver");
}Remarks
The handle returned is valid until the DRV_SST38_Close routine is called.
If the driver has already been opened, it should not be opened again.