DRV_SST38_Status Function
C
SYS_STATUS DRV_SST38_Status( const SYS_MODULE_INDEX drvIndex )Summary
Gets the current status of the SST38 driver module.
Description
This routine provides the current status of the SST38 driver module.
Preconditions
Function DRV_SST38_Initialize should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| drvIndex | Identifier for the instance used to initialize driver |
Returns
SYS_STATUS_READY - Indicates that the driver is ready and accept requests for new operations.
SYS_STATUS_UNINITIALIZED - Indicates the driver is not initialized.
SYS_STATUS_BUSY - Indicates the driver is in busy state.
Example
SYS_STATUS Status;
Status = DRV_SST38_Status(DRV_SST38_INDEX);
if (status == SYS_STATUS_READY)
{
printf("SST38 driver is initialized and ready to accept requests.");
}Remarks
None.