DRV_AT25_Close Function
C
void DRV_AT25_Close( const DRV_Handle handle )Summary
Closes the opened-instance of the AT25 driver.
Description
This routine closes opened-instance of the AT25 driver, invalidating the handle. A new handle must be obtained by calling DRV_AT25_Open before the caller may use the driver again.
Precondition
DRV_AT25_Open must have been called to obtain a valid opened device handle.
Parameters
| Param | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
Returns
None.
Example
// 'handle', returned from the DRV_AT25_Open DRV_AT25_Close(handle);
Remarks
None.