DRV_AT25_Status Function
C
SYS_STATUS DRV_AT25_Status( const SYS_MODULE_INDEX drvIndex )Summary
Gets the current status of the AT25 driver module.
Description
This routine provides the current status of the AT25 driver module.
Preconditions
Function DRV_AT25_Initialize should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| drvIndex | Identifier for the instance used to initialize driver |
Returns
SYS_STATUS_READY - Indicates that the driver is ready and accept requests for new operations.
SYS_STATUS_UNINITIALIZED - Indicates the driver is not initialized.
Example
SYS_STATUS status;
status = DRV_AT25_Status(DRV_AT25_INDEX);
if (status == SYS_STATUS_READY)
{
// AT25 driver is initialized and ready to accept requests.
}Remarks
None.