DRV_SST26_Status Function
C
SYS_STATUS DRV_SST26_Status( const SYS_MODULE_INDEX drvIndex );Summary
Gets the current status of the SST26 driver module.
Description
This routine provides the current status of the SST26 driver module.
Preconditions
Function DRV_SST26_Initialize should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| drvIndex | Identifier for the instance used to initialize driver |
Returns
SYS_STATUS_READY - Indicates that the driver is ready and accept requests for new operations.
SYS_STATUS_UNINITIALIZED - Indicates the driver is not initialized.
SYS_STATUS_BUSY - Indicates the driver is in busy state.
Example
SYS_STATUS Status;
Status = DRV_SST26_Status(DRV_SST26_INDEX);
if (status == SYS_STATUS_READY)
{
// SST26 driver is initialized and ready to accept requests.
}Remarks
None.