1.3.1.4.2 EMU_EEPROM_StatusGet Function
1.3.1.4.2 C
EMU_EEPROM_STATUS EMU_EEPROM_StatusGet( void )
1.3.1.4.2 Summary
Gets the current status of the EEPROM Emulator library.
1.3.1.4.2 Description
This routine provides the status of the EEPROM Emulator library.
1.3.1.4.2 Precondition
Function EMU_EEPROM_Initialize should have been called before calling this function.
1.3.1.4.2 Parameters
None.
1.3.1.4.2 Returns
EMU_EEPROM_STATUS - Enum of type EMU_EEPROM_STATUS. Status code indicating the status of the operation.
1.3.1.4.2 Example
if (EMU_EEPROM_StatusGet() == EMU_EEPROM_STATUS_ERR_BAD_FORMAT)
{
//Format the EEPROM Emulation memory if the initialization failed
EMU_EEPROM_FormatMemory();
}
1.3.1.4.2 Remarks
None.