1.3.1.4.1 EMU_EEPROM_Initialize Function

1.3.1.4.1 C

SYS_MODULE_OBJ EMU_EEPROM_Initialize(const SYS_MODULE_INDEX drvIndex, const SYS_MODULE_INIT* const init)

1.3.1.4.1 Summary

Initializes the EEPROM Emulator library.

1.3.1.4.1 Description

Initializes the emulated EEPROM memory space. If the emulated EEPROM memory has not been previously initialized, it must be explicitly formatted using EMU_EEPROM_EraseMemory(). The EEPROM memory space will not be automatically erased by the initialization function, so that partial data may be recovered by the user application manually if the service is unable to initialize successfully.

1.3.1.4.1 Precondition

None.

1.3.1.4.1 Parameters

ParametersDescription
drvIndexIdentifier for the instance to be initialized
initPointer to the init data structure containing any data necessary to initialize the driver

1.3.1.4.1 Returns

If successful, returns a valid handle to a driver instance object. Otherwise, it returns SYS_MODULE_OBJ_INVALID.

1.3.1.4.1 Example

// The following code snippet shows an example I2C driver initialization.

sysObj.libEMULATED_EEPROM0 = EMU_EEPROM_Initialize(EMULATED_EEPROM0, (SYS_MODULE_INIT *)NULL);

1.3.1.4.1 Remarks

This routine must be called before any other EEPROM Emulation library routine is called. This routine should only be called once during system initialization.