1.3.1.4.10 EMU_EEPROM_STATUS Enum
1.3.1.4.10 C
typedef enum
{
/* Operation is successful or EEPROM Emulator is successfully initialized. */
EMU_EEPROM_STATUS_OK,
/* No EEPROM section has been allocated in the device */
EMU_EEPROM_STATUS_ERR_NO_MEMORY,
/* If an address outside the valid emulated EEPROM memory space was supplied */
EMU_EEPROM_STATUS_ERR_BAD_ADDRESS,
/* Emulated EEPROM memory is corrupt or not formatted or is incompatible with this version or scheme of the EEPROM emulator*/
EMU_EEPROM_STATUS_ERR_BAD_FORMAT,
/* Emulated EEPROM is not initialized */
EMU_EEPROM_STATUS_ERR_NOT_INITIALIZED
}EMU_EEPROM_STATUS;
1.3.1.4.10 Summary
Identifies the current status/state of EEPROM operation.
1.3.1.4.10 Description
This enumeration identifies the current status/state of the EEPROM operation.
1.3.1.4.10 Remarks
None.