1.2.5.4.2 SYS_DEBUG_Status Function

1.2.5.4.2 C

SYS_STATUS SYS_DEBUG_Status ( SYS_MODULE_OBJ object )

1.2.5.4.2 Summary

Returns status of the specific instance of the debug service module.

1.2.5.4.2 Description

This function returns the status of the specific debug service module instance.

1.2.5.4.2 Precondition

The SYS_DEBUG_Initialize function should have been called before calling this function.

1.2.5.4.2 Parameters

ParametersDescription
objectDebug module object handle, returned from SYS_DEBUG_Initialize

1.2.5.4.2 Returns

SYS_STATUS_READY - Indicates that the module is running and ready to service requests. Any value greater than SYS_STATUS_READY is also a normal running state in which the module is ready to accept new operations.

SYS_STATUS_BUSY - Indicates that the module is busy with a previous system level operation.

SYS_STATUS_ERROR - Indicates that the module is in an error state. Any value less than SYS_STATUS_ERROR is also an error state.

SYS_STATUS_UNINITIALIZED - Indicates that the module has not been initialized.

1.2.5.4.2 Example

SYS_MODULE_OBJ object; // Returned from SYS_CONSOLE_Initialize
SYS_STATUS debugStatus;

debugStatus = SYS_DEBUG_Status (object);

if (debugStatus == SYS_STATUS_READY)
{
    // Debug service is initialized and ready to accept requests.
}

1.2.5.4.2 Remarks

None.