1.1.7.4.15 DRV_SDSPI_Read Function
C
void DRV_SDSPI_Read
(
const DRV_HANDLE handle,
DRV_SDSPI_COMMAND_HANDLE* commandHandle,
void* targetBuffer,
uint32_t blockStart,
uint32_t nBlock
)Summary
This routine provides interface to the file system to perform a media read operation in Synchronous mode of the SDSPI driver.
Description
This function is internally used by the file system.
Preconditions
The DRV_SDSPI_Initialize routine must have been called. The DRV_SDSPI_Open must have been called to obtain a valid opened device handle.
Parameters
| Parameters | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open function |
| commandHandle | Pointer to an argument that will contain the return buffer handle |
| targetBuffer | Buffer into which the data read from the SD card will be placed |
| blockStart | Start block address of the SD card from where the read should begin |
| nBlock | Total number of blocks to be read |
Returns
The buffer handle is returned in the commandHandle argument. It will be DRV_SDSPI_COMMAND_HANDLE_INVALID if the request was not successful.
Example
None.
Remarks
This function is internally used by the file system.