1.1.7.4.12 DRV_SDSPI_GeometryGet Function

C

SYS_MEDIA_GEOMETRY* DRV_SDSPI_GeometryGet
(
    const DRV_HANDLE handle
)

Summary

Returns the geometry of the device.

Description

This API gives the following geometrical details of the SD card.

  • Media Property

  • Number of Read/Write/Erase regions in the SD card

  • Number of Blocks and their size in each region of the device

Precondition

The DRV_SDSPI_Initialize routine must have been called for the specified SDSPI driver instance.

The DRV_SDSPI_Open routine must have been called to obtain a valid opened device handle.

Parameters

ParametersDescription
handleA valid open-instance handle, returned from the driver's open function

Returns

SYS_MEDIA_GEOMETRY - Pointer to structure which holds the media geometry information.

Example

SYS_MEDIA_GEOMETRY * SDSPIGeometry;
uint32_t readBlockSize, writeBlockSize, eraseBlockSize;
uint32_t nReadBlocks, nReadRegions, totalSize;

// mySDSPIHandle is the handle returned by the DRV_SDSPI_Open function.
SDSPIGeometry = DRV_SDSPI_GeometryGet(mySDSPIHandle);

readBlockSize = SDSPIGeometry->geometryTable->blockSize;
nReadBlocks = SDSPIGeometry->geometryTable->numBlocks;
nReadRegions = SDSPIGeometry->numReadRegions;

writeBlockSize = (SDSPIGeometry->geometryTable +1)->blockSize;
eraseBlockSize = (SDSPIGeometry->geometryTable +2)->blockSize;

totalSize = readBlockSize * nReadBlocks * nReadRegions;

Remarks

Refer to the sys_media.h for definition of SYS_MEDIA_GEOMETRY.