1.1.7.4.7 DRV_SDSPI_AsyncRead Function
C
void DRV_SDSPI_AsyncRead (
const DRV_HANDLE handle,
DRV_SDSPI_COMMAND_HANDLE* commandHandle,
void* targetBuffer,
uint32_t blockStart,
uint32_t nBlocks
)Summary
Reads blocks of data from the specified block address of the SD card.
Description
This function schedules a non-blocking read operation for reading blocks of data from the SD card. The function returns with a valid buffer handle in the commandHandle argument if the read request was scheduled successfully. The function adds the request to the hardware instance queue and returns immediately. While the request is in the queue, the application buffer is owned by the driver and should not be modified. The function returns DRV_SDSPI_COMMAND_HANDLE_INVALID in the commandHandle argument under the following circumstances:
if the driver handle is invalid
if the target buffer pointer is NULL
if the number of blocks to be read is zero or more than the actual number of blocks available
Error during the read operation
Precondition
The DRV_SDSPI_Initialize routine must have been called for the specified SDSPI driver instance.
DRV_SDSPI_Open must have been called to obtain a valid opened device handle.
Parameters
| Parameters | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open function |
| commandHandle | Pointer to an argument that will contain the return buffer handle |
| targetBuffer | Buffer into which the data read from the SD card will be placed |
| blockStart | Starting block address of the SD card from where the read should begin |
| nBlock | Total number of blocks to be read |
Returns
The buffer handle is returned in the commandHandle argument. It will be DRV_SDSPI_COMMAND_HANDLE_INVALID if the request was not successful.
Example
uint8_t CACHE_ALIGN myBuffer[MY_BUFFER_SIZE]; // address should be block aligned. uint32_t blockStart = 0x00; uint32_t nBlock = 2; DRV_SDSPI_COMMAND_HANDLE commandHandle; MY_APP_OBJ myAppObj; // Event is received when // the buffer is processed. void APP_SDSPIEventHandler( DRV_SDSPI_EVENT event, DRV_SDSPI_COMMAND_HANDLE commandHandle, uintptr_t contextHandle ) { // contextHandle points to myAppObj. switch(event) { case DRV_SDSPI_EVENT_COMMAND_COMPLETE: { // This means the data was transferred successfully break; } case DRV_SDSPI_EVENT_COMMAND_ERROR: { // Error handling here break; } default: { break; } } } // mySDSPIHandle is the handle returned // by the DRV_SDSPI_Open function. // Client registers an event handler with driver DRV_SDSPI_EventHandlerSet(mySDSPIHandle, APP_SDSPIEventHandler, (uintptr_t)&myAppObj); DRV_SDSPI_AsyncRead(mySDSPIHandle, &commandHandle, &myBuffer[0], blockStart, nBlock); if(commandHandle == DRV_SDMMC_COMMAND_HANDLE_INVALID) { // Error handling here } else { // Read Successfully queued }
Remarks
None.