DRV_SST26_GeometryGet Function

C

bool DRV_SST26_GeometryGet( const DRV_HANDLE handle, SST26_GEOMETRY *geometry );

Summary

Returns the geometry of the device.

Description

This API gives the following geometrical details of the SST26 Flash:

  • Number of Read/Write/Erase Blocks and their size in each region of the device
  • Flash block start address

Precondition

The DRV_SST26_Open() routine must have been called for the specified SST26 driver instance.

Parameters

ParametersDescription
handleA valid open-instance handle, returned from the driver's open routine
*geometry_tablePointer to Flash device geometry table instance

Returns

True - If able to get the geometry details of the Flash.

False - If read device id fails.

Example

DRV_HANDLE handle; // Returned from DRV_SST26_Open

DRV_SST26_GEOMETRY sst26FlashGeometry;

uint32_t readBlockSize, writeBlockSize, eraseBlockSize;
uint32_t nReadBlocks, nReadRegions, totalFlashSize;

DRV_SST26_GeometryGet(handle, &sst26FlashGeometry);

readBlockSize = sst26FlashGeometry.read_blockSize;
nReadBlocks = sst26FlashGeometry.read_numBlocks;
nReadRegions = sst26FlashGeometry.numReadRegions;

writeBlockSize = sst26FlashGeometry.write_blockSize;
eraseBlockSize = sst26FlashGeometry.erase_blockSize;

totalFlashSize = readBlockSize * nReadBlocks * nReadRegions;

Remarks

This API is more useful when used to interface with Memory driver.