1.1.10.4.19 DRV_USART_BUFFER_EVENT Enum
1.1.10.4.19 C
typedef enum
{
/* The buffer is pending to be serviced */
DRV_USART_BUFFER_EVENT_PENDING = 0,
/* All data from or to the buffer was transferred successfully. */
DRV_USART_BUFFER_EVENT_COMPLETE = 1,
/* Transfer Handle given is expired. It means transfer
is completed but with or without error is not known. */
DRV_USART_BUFFER_EVENT_HANDLE_EXPIRED = 2,
/* There was an error while processing the buffer transfer request. */
DRV_USART_BUFFER_EVENT_ERROR = -1,
/* Transfer Handle given is invalid */
DRV_USART_BUFFER_EVENT_HANDLE_INVALID = -2
} DRV_USART_BUFFER_EVENT;
1.1.10.4.19 Summary
Identifies the possible events that can result from a buffer add request.
1.1.10.4.19 Description
This enumeration identifies the possible events that can result from a buffer add request caused by the client calling either the DRV_USART_ReadBufferAdd or DRV_USART_WriteBufferAdd functions.
1.1.10.4.19 Remarks
One of these values is passed in the "event" parameter of the event handling callback function that the client registered with the driver by calling the DRV_USART_BufferEventHandlerSet function when a buffer transfer request is completed.