DRV_SST38_Close Function

C

void DRV_SST38_Close( const DRV_HANDLE handle )

Summary

Closes an opened-instance of the SST38 driver.

Description

This routine closes an opened-instance of the SST38 driver, invalidating the handle.

Precondition

DRV_SST38_Open must have been called to obtain a valid opened device handle.

Parameters

ParametersDescription
handleA valid open-instance handle, returned from the driver's open routine

Returns

None.

Example

DRV_HANDLE handle; // Returned from DRV_SST38_Open

DRV_SST38_Close(handle);

Remarks

After calling this routine, the handle passed in "handle" must not be used with any of the remaining driver routines. A new handle must be obtained by calling DRV_SST38_Open before the caller may use the driver again.

Usually there is no need for the driver client to verify that the Close operation has completed.