DRV_SST38_Status Function

C

SYS_STATUS DRV_SST38_Status( const SYS_MODULE_INDEX drvIndex )

Summary

Gets the current status of the SST38 driver module.

Description

This routine provides the current status of the SST38 driver module.

Preconditions

Function DRV_SST38_Initialize should have been called before calling this function.

Parameters

ParametersDescription
drvIndexIdentifier for the instance used to initialize driver

Returns

SYS_STATUS_READY - Indicates that the driver is ready and accept requests for new operations.

SYS_STATUS_UNINITIALIZED - Indicates the driver is not initialized.

SYS_STATUS_BUSY - Indicates the driver is in busy state.

Example

SYS_STATUS Status;

Status = DRV_SST38_Status(DRV_SST38_INDEX);

if (status == SYS_STATUS_READY)
{
    printf("SST38 driver is initialized and ready to accept requests.");
}

Remarks

None.