DRV_SST38_PageWrite Function

C

bool DRV_SST38_PageWrite( const DRV_HANDLE handle, void *tx_data, uint32_t address )

Summary

Writes one page of data starting at the specified address.

Description

This function schedules a blocking write operation for writing maximum one page of data into Flash memory.

Preconditions

The DRV_SST38_Open() routine must have been called for the specified SST38 driver instance.

The Flash address location which has to be written, must have been erased before using the SST38_xxxErase() routine.

The Flash address has to be a Page aligned address.

Parameters

ParametersDescription
handleA valid open-instance handle, returned from the driver's open routine
tx_dataThe source buffer containing data to be programmed into SST38 Flash
addressWrite memory start address from where the data should be written

Returns

  • True:

    • If the write request is successfully sent to the Flash

  • False:

    • If Write enable fails before sending sector erase command to Flash

    • If write command itself fails

Example

#define PAGE_SIZE    256
#define BUFFER_SIZE  1024
#define MEM_ADDRESS  0x0

DRV_HANDLE handle;
uint8_t CACHE_ALIGN writeBuffer[BUFFER_SIZE];
bool status = false;

if(false == DRV_SST38_SectorErase(handle))
{
    printf("Error handling here");
}

for (uint32_t j = 0; j < BUFFER_SIZE; j += PAGE_SIZE)
{
    if (DRV_SST38_PageWrite(handle, (void *)&writeBuffer[j], (MEM_ADDRESS + j)) == false)
    {
        status = false;
        break;
    }

    status = true;
}

if(status == false)
{
    printf("Error handling here");
}

Remarks

None.