8.4 DTS Settings for SPI Interface
The WILCS02 supports the SDIO-SPI mode to communicate
with host platforms using the MMC over SPI interface. To work with SDIO-SPI mode,
the
cs-gpios and intr-gpios of SPI in the DTS file
need to be set accordingly. cs-gpiosis the SPI Chip Select GPIO pin configurationintr-gpiosis the SPI IRQN pin configuration
Interrupt-parent and interrupts can be set to
any GPIO pin for the card detect(cd) IRQ of MMC-SPI because WILCS02 does not support the MMC-SPI card detect. The definition of this
pin is just for the normal working of the MMC-SPI. The following is an example of the MMC-SPI DTS setting on the SAMA7D27-SOM1-EK
platform.
&spi6 {
#address-cells = <1>;
#size-cells = <0>;
cs-gpios = <&pioA PIN_PD0 GPIO_ACTIVE_LOW>;
cap-sd-highspeed;
status = "okay";
wilc_spi@1 {
compatible = "microchip,wilc1000", "microchip,wilc3000", "mmc-spi-slot";
spi-max-frequency = <40000000>;
reg = <0>;
interrupt-parent = <&pioA>;
interrupts = <PIN_PA25 0>;
intr-gpios = <&pioA PIN_PB0 0>;
status = "okay";
};
};